NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
we are strugling in our project that is now in a trial with the customer and I need your tech support to provide the information on the way to increase the TX power to maximum. We are now seeing a -30dbm directly from the STM32WLE5JCI6 pinout RFO_HP...
Hello,I'm currently working on an application that integrates the LoRaWAN stack (version 2.1.0), and has to use USART2 to send/receive data. USART2 is already used by the trace utility, to send trace messages. I activated RX on interruption by callin...
We are working with android and there are multiple problems it is causing us with its Service Changed characteristic.Is there a way it will not be created? Some chcekbox in CubeMx or else?Cheers!
Hi,We are designing ou custom Lora application based on the STM32WLE5CCU6 MCU.1- We would like to know if there is an eval board that can be used in manufacturing tests to perform a pingpong communication test (between our custom board and the eval b...
Hello,Not a question but since I searched for this information and could not locate it anywhere, I post it here to maybe help others.When calling aci_gatt_init(void), it is said that the Service Changed Characteristic is added automatically. /** * @...
Hi I am using Nucleo-WL55JC1 boards with STMCubeWL firmware version 1.2.0. I have problem with multicast group FUOTA on Lorawan that send package to only one device even though there are more devices in the group. All devices work in class C.Thank yo...
I have designed a custom developer board based on STM32WB55CGU6. I have both JTAG and SWD pins on the board. None of them works when I try to connect the board to the STLINK v3MINIE. Except any hardware issues, what else do you suggest for the very f...
I have successfully implemented a ZigBee coordinator/router with an on/off-server-cluster based on a STM32WB5MMG module.My application is able to form a network and automatically allows certain off-the-shelf ZigBee On/Off-Clients to join the network ...
I am using a "Sigfox AT Slave" example project. When I type the AT command to get the Sigfox ID or PAC I get an "OK" message as if the command worked, but the ID or PAC do not appear.