cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX on STM32H7S78 — Screen Flickering, Missing Text, Mixed Screens During Navigation

Mehulrana511
Associate III
Software:
TouchGFX Designer + STM32CubeMX + STM32CubeIDE

Problems observed:
- Screen flickers randomly especially during screen transitions.
- UI text disappears or becomes invisible after returning to a screen.
- Mixed or corrupted screens — elements from previous screen appear on the next one.
- Sometimes partial or outdated frame buffer content is displayed.
These issues occur consistently when navigating between screens, I attached video for your reference.
 
TouchGFX Environment:
- LTDC enabled, RGB interface, external display 7” TFT
- TouchGFX task priority: Normal
- TouchGFX task stack size: 4096 bytes
- Running under FreeRTOS

What I have already tried:
- I have tested the following but issue still persists:
- Increased TouchGFX task stack (4096 → 8192)
- Ensured LTDC clocks are correct
- Ensured invalidate() is called after UI updates

Looking forward to your further guidance.

Best regards,
Mehul Rana
 
 
(Virus scan in progress ...)
0 REPLIES 0