2025-09-08 7:20 AM
I want to use TouchGFX Designer in a Project for which no .ioc file exists, but generating code in the Designer fails because of the missing .ioc file.
Is it possible to work around this? If I need to use a dummy .ioc file, which settings are relevant for the Designer?
Solved! Go to Solution.
2025-09-08 7:30 AM - edited 2025-09-08 7:34 AM
Hello,
I'm not TouchGFX expert, but it seems the ioc file is needed for the hardware configuration: LCD, RAM etc.. when generating the code for the target.
This is an example of a log while generating a code for a board where the ioc file is missing:
So it's is generating a code for the target (MCU) meaning that it needs the hardware config and not the simulator (your PC).
2025-09-08 7:30 AM - edited 2025-09-08 7:34 AM
Hello,
I'm not TouchGFX expert, but it seems the ioc file is needed for the hardware configuration: LCD, RAM etc.. when generating the code for the target.
This is an example of a log while generating a code for a board where the ioc file is missing:
So it's is generating a code for the target (MCU) meaning that it needs the hardware config and not the simulator (your PC).