2022-04-27 1:11 AM
Hi Community,
When I use the Touch GFX from software packs in STM32CubeIDE and generate the project, I am getting the following errors. So, anyone is having idea how to solve this?
1) region `RAM' overflowed by 1168976 bytes.
2) touchgfx_ide_new.elf section `Video_RGB_Buffer' will not fit in region `RAM'.
Thank you.
Vins.
Solved! Go to Solution.
2022-04-28 12:03 AM
Hi guys,
It's correct that the code generated by 4.19.1 Generator (through CubeMX/CubeIDE) now has instrumentation that allows you to place the buffers where you want to (by making appropriate modifications in your linker script). So, if you're using an older version you'll have to make modifications to the generated code (which would get overwritten upon next code generation from CubeMX). Here's the change:
LOCATION_PRAGMA("Video_RGB_Buffer")
uint32_t videoRGBBuffer[...calculated size...] LOCATION_ATTRIBUTE("Video_RGB_Buffer");As such, if you're just using CubeMX/CubeIDE to create a custom project, you will not have a linker script for your board that has any reference to the Video Buffer (You can get inspiration from one of our board packs through the designer that supports video).
You should be able to find some information here about the matter:
Video Decoding | TouchGFX Documentation
Here's an example of how to place the buffer in SDRAM for CubeIDE. In this example, the SDRAM region (@ 0xC00FF000) has been defined after the framebuffer which is not allocated, but referenced by address (start of SDRAM @ 0xC0000000).
MEMORY
{
...
SDRAM (xrw) : ORIGIN = 0xC00FF000, LENGTH = 8M
}
BufferSection :
{
*(Video_RGB_Buffer Video_RGB_Buffer.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x4);
} >SDRAMAnd here's the .map file for the above configuration:
BufferSection 0x00000000c00ff000 0x1c200
*(Video_RGB_Buffer Video_RGB_Buffer.*)
Video_RGB_Buffer
0x00000000c00ff000 0x1c200 Application/User/TouchGFX/target/generated/TouchGFXGeneratedHAL.o
0x00000000c00ff000 videoRGBBufferFurther Improvement in next version:
The next version of TouchGFX will support a new configuration for MDK-ARM compilers that might otherwise try to write zeros to the Video buffer SDRAM region before it's initialized, causing a crash.
/Martin
2022-04-27 7:01 AM
You can't use more RAM than you have. That should be straightforward.
Put the buffer into external RAM if available on the hardware.
2022-04-27 7:19 AM
Hello,
Please use TouchGFX v4.19.1. It relocates video buffer in SDRAM.
2022-04-27 10:04 PM
@Community member Hi, I am directly not using v4.19.1 designer. I am using STM32CubeIDE in this activating Touch GFX v4.19.1 designer. Getting the same error.
2022-04-28 12:03 AM
Hi guys,
It's correct that the code generated by 4.19.1 Generator (through CubeMX/CubeIDE) now has instrumentation that allows you to place the buffers where you want to (by making appropriate modifications in your linker script). So, if you're using an older version you'll have to make modifications to the generated code (which would get overwritten upon next code generation from CubeMX). Here's the change:
LOCATION_PRAGMA("Video_RGB_Buffer")
uint32_t videoRGBBuffer[...calculated size...] LOCATION_ATTRIBUTE("Video_RGB_Buffer");As such, if you're just using CubeMX/CubeIDE to create a custom project, you will not have a linker script for your board that has any reference to the Video Buffer (You can get inspiration from one of our board packs through the designer that supports video).
You should be able to find some information here about the matter:
Video Decoding | TouchGFX Documentation
Here's an example of how to place the buffer in SDRAM for CubeIDE. In this example, the SDRAM region (@ 0xC00FF000) has been defined after the framebuffer which is not allocated, but referenced by address (start of SDRAM @ 0xC0000000).
MEMORY
{
...
SDRAM (xrw) : ORIGIN = 0xC00FF000, LENGTH = 8M
}
BufferSection :
{
*(Video_RGB_Buffer Video_RGB_Buffer.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x4);
} >SDRAMAnd here's the .map file for the above configuration:
BufferSection 0x00000000c00ff000 0x1c200
*(Video_RGB_Buffer Video_RGB_Buffer.*)
Video_RGB_Buffer
0x00000000c00ff000 0x1c200 Application/User/TouchGFX/target/generated/TouchGFXGeneratedHAL.o
0x00000000c00ff000 videoRGBBufferFurther Improvement in next version:
The next version of TouchGFX will support a new configuration for MDK-ARM compilers that might otherwise try to write zeros to the Video buffer SDRAM region before it's initialized, causing a crash.
/Martin