cancel
Showing results for 
Search instead for 
Did you mean: 

F429 Disco USB Stick problem

warcatz
Associate II
Posted on October 13, 2013 at 19:50

Hi :)

As usual 'Murphy law' i get little problem ....

I have connect 3 different USB Stick on 3 Different F429 Disco Board though the microSD connector with no results.

I then tried with a USB connector directly connected to the USB dedicated pins with the same no results :(

Is it something special to do to made it work ??

From the docs i doesn't see anything special to do for the micro usb port , i have think it will

be functional directly with the provided demo ...

I formatted them in fat16 and fat32 for be sure and they are 1,2 and 4Gb.

Cheers.

#discovery #stm32f429 #lcd-tft
This discussion is locked. Please start a new topic to ask your question.
22 REPLIES 22
mitcharnaud31
Associate II
Posted on October 16, 2013 at 20:52

I tried to put 8Mhz on the HSE, same result.

OK, I will open a new topic about USB device VCP.

Thanks for your help.
mitcharnaud31
Associate II
Posted on October 16, 2013 at 21:41

Do you mean ''it is working'' ?

Posted on October 16, 2013 at 21:56

Do you mean ''it is working'' ?

It appears to be functioning.

Edit#1 Seems to crash when disconnected, will need to dig into that.

Edit#2 See how to resolve that
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..