STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

How to draw a line with finger?

Hi,How can i draw a line on my display touchscreen with my finger.I have used Graph widget before,but the coordinate point must be monotone increasing。Could i use the method for QrCode,and could you write an example for this。Thanks�?�?�?Best regards​

Jack li1 by Associate III
  • 1255 Views
  • 3 replies
  • 1 kudos

STM32F769i-Discovery video mode examples

Looking through the video mode examples that use SDRAM, I see that in BSP_SDRAM_MspInit() a DMA channel is initialised but as far as I can see none of the examples makes use of DMA.Is this a fundamental requirement to operate the SDRAM with the LTDC ...

CubeMX, Atollic, TouchGFX framework Directory

I have a STM32F746G-Discovery board and the CubeMX and TouchGFX project setup in Atollic.Much of it is functioning. However when I went to edit in the TouchGFX​ Designer, I had compilation errors when generating code.It seems the Directory  \STM32F74...

MEder by Associate III
  • 1125 Views
  • 4 replies
  • 0 kudos

OV2640 YCbCr 4:2:2 + DMA2D

I have a few questions about DMA2D.I do not want to create separate topics for each question, so I will be glad if you answer at least one of them.1) I successfully get a picture in RGB565, but as soon as I choose YCbCr, it turns out a bad picture (i...

0690X000006Dl8qQAC.jpg

Can TouchGFX and CubeMX drive 1024x600 display?

Hello!I try to change display resolution in cubeMX for project based on stm32f429zit6On page Graphics->Parameter settings I try to change width. Maximum allowed change - to 1000. If I set 1001 or more - changings not saves. I try to disable checkin...

EEuge by Senior
  • 801 Views
  • 1 replies
  • 0 kudos

how is the Touch GFX supposed to work ?

I see the icon top right corner, generate code. But when I press it nothing happens, it becomes like inactive grayed out like it is doing something for a few seconds but nothing happens.Is this because used Windows 7, do I need Win 10 ? Is this suppo...

MNapi by Senior III
  • 1746 Views
  • 6 replies
  • 0 kudos

STM32F439BG\LCD Display

Hello,I want to use STM32F439BG in my product.I am Confusing about the LCD Display.I want to use LCD - Capacitive Touch, 5.7 Inch, RGB (R-8, G-8, B-8, HSYNC, VSYNC, CLK, DE) which will be connected with STM32F439BG.Please suggest the LCD Compatible w...

ABora.4 by Associate III
  • 1253 Views
  • 3 replies
  • 0 kudos