STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX: How to enable an external data reader?

I am implementing a low cost custom TouchGFX project using a stm342G071 and an ILI9488 based display. For the ILI9488 driver I need the touchGFX framebuffer in RGB888 format.This works ok if I keep the image data in internal flash but I need to put ...

TMack.1 by Associate II
  • 2137 Views
  • 1 replies
  • 0 kudos

How to set Y-Axis Labels scale?

Hi All,I have a question about dynamic graph widget in TouchGFX.How can I set different scale for Y-Axis labels?For example, I have data values that goes from 0 to 20000 so I set the Value Range from 0 to 20000. But I want to display Y-Axis labels fr...

nikof by Associate II
  • 2218 Views
  • 3 replies
  • 0 kudos

RadioButton and RadioButtonGroups

I see that you can place multiple radio buttons on a screen and they work as expected. (all the buttons)Can you have multiple radio button groups on the same screen? see image below can I have group 1 work independently to group 2How can I achieve th...

0693W00000UnOUDQA3.png

FontFlashSection in memory mapped SDRAM

Hello,My architecture is based on STM32H750 with an external memory mapped SDRAM used to store the framebuffer and -willingly- used to store at runtime assest such as texts fonts and images.I’ve modified my linker file to:MEMORY { FWINFO (rx) : O...

0693W00000Unz4CQAR.jpg 0693W00000Unz4RQAR.jpg
MArri.1 by Associate II
  • 3404 Views
  • 5 replies
  • 0 kudos