2025-08-29 6:21 AM
Hi, I'm using 3 channels of ADC4 with GPDMA1 (channel 4) in secure world of a TrustZone-project and the DMA-buffer stays always 0. The same ADC/DMA-configuration with the same application code (all mnus the security aspects) are working fine without TrustZone on the same hardware. I set the DMA-channel and the ADC-channel to secure and privileged, also the SAU-configuration for these peripherals is secure, the DMA-interrupt (circular) is triggered and calling HAL_ADC_ConvCpltCallback but there's nothing inside the DMA-buffer (which is defined as volatile inside a secure and privileged SRAM-area). I've tried different ADC conversion rates, clock rates and clock sources, checked for errors (especially overruns) and secure faults (with GTZC), there's absolutely nothing. I guess it must have something to do with secure/privileged areas or peripherals but since all the parts are secure and privileged I don't know what it could be. I'd be thankful for any suggestions; here is my ADC DMA-initialization code:
void MX_ADC4_Init(void)
{
/* USER CODE BEGIN ADC4_Init 0 */
/* USER CODE END ADC4_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC4_Init 1 */
/* USER CODE END ADC4_Init 1 */
/** Common config
*/
hadc4.Instance = ADC4;
hadc4.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV64;
hadc4.Init.Resolution = ADC_RESOLUTION_12B;
hadc4.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc4.Init.ScanConvMode = ADC4_SCAN_ENABLE;
hadc4.Init.EOCSelection = ADC_EOC_SEQ_CONV;
hadc4.Init.LowPowerAutoPowerOff = ADC_LOW_POWER_NONE;
hadc4.Init.LowPowerAutoWait = DISABLE;
hadc4.Init.ContinuousConvMode = ENABLE;
hadc4.Init.NbrOfConversion = 3;
hadc4.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc4.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc4.Init.DMAContinuousRequests = ENABLE;
hadc4.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
hadc4.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
hadc4.Init.SamplingTimeCommon1 = ADC4_SAMPLETIME_7CYCLES_5;
hadc4.Init.SamplingTimeCommon2 = ADC4_SAMPLETIME_1CYCLE_5;
hadc4.Init.OversamplingMode = ENABLE;
hadc4.Init.Oversampling.Ratio = ADC_OVERSAMPLING_RATIO_2;
hadc4.Init.Oversampling.RightBitShift = ADC_RIGHTBITSHIFT_1;
hadc4.Init.Oversampling.TriggeredMode = ADC_TRIGGEREDMODE_SINGLE_TRIGGER;
if (HAL_ADC_Init(&hadc4) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_9;
sConfig.Rank = ADC4_REGULAR_RANK_1;
sConfig.SamplingTime = ADC4_SAMPLINGTIME_COMMON_1;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_10;
sConfig.Rank = ADC4_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_11;
sConfig.Rank = ADC4_REGULAR_RANK_3;
if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC4_Init 2 */
/* USER CODE END ADC4_Init 2 */
}
void HAL_ADC_MspInit(ADC_HandleTypeDef* adcHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
DMA_NodeConfTypeDef NodeConfig= {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
if(adcHandle->Instance==ADC4)
{
/* USER CODE BEGIN ADC4_MspInit 0 */
/* USER CODE END ADC4_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_ADCDAC;
PeriphClkInit.AdcDacClockSelection = RCC_ADCDACCLKSOURCE_HCLK;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/* ADC4 clock enable */
__HAL_RCC_ADC4_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/**ADC4 GPIO Configuration
PA4 ------> ADC4_IN9
PA5 ------> ADC4_IN10
PA6 ------> ADC4_IN11
*/
GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* ADC4 DMA Init */
/* GPDMA1_REQUEST_ADC4 Init */
NodeConfig.NodeType = DMA_GPDMA_LINEAR_NODE;
NodeConfig.SrcSecure = DMA_CHANNEL_SRC_SEC;
NodeConfig.DestSecure = DMA_CHANNEL_DEST_SEC;
NodeConfig.Init.Request = GPDMA1_REQUEST_ADC4;
NodeConfig.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
NodeConfig.Init.Direction = DMA_PERIPH_TO_MEMORY;
NodeConfig.Init.SrcInc = DMA_SINC_FIXED;
NodeConfig.Init.DestInc = DMA_DINC_INCREMENTED;
NodeConfig.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_HALFWORD;
NodeConfig.Init.DestDataWidth = DMA_DEST_DATAWIDTH_HALFWORD;
NodeConfig.Init.SrcBurstLength = 1;
NodeConfig.Init.DestBurstLength = 1;
NodeConfig.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0;
NodeConfig.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
NodeConfig.Init.Mode = DMA_NORMAL;
NodeConfig.TriggerConfig.TriggerPolarity = DMA_TRIG_POLARITY_MASKED;
NodeConfig.DataHandlingConfig.DataExchange = DMA_EXCHANGE_NONE;
NodeConfig.DataHandlingConfig.DataAlignment = DMA_DATA_RIGHTALIGN_ZEROPADDED;
NodeConfig.SrcSecure = DMA_CHANNEL_SRC_SEC;
NodeConfig.DestSecure = DMA_CHANNEL_DEST_SEC;
if (HAL_DMAEx_List_BuildNode(&NodeConfig, &Node_GPDMA1_Channel4) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMAEx_List_InsertNode(&List_GPDMA1_Channel4, NULL, &Node_GPDMA1_Channel4) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMAEx_List_SetCircularMode(&List_GPDMA1_Channel4) != HAL_OK)
{
Error_Handler();
}
handle_GPDMA1_Channel4.Instance = GPDMA1_Channel4;
handle_GPDMA1_Channel4.InitLinkedList.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
handle_GPDMA1_Channel4.InitLinkedList.LinkStepMode = DMA_LSM_FULL_EXECUTION;
handle_GPDMA1_Channel4.InitLinkedList.LinkAllocatedPort = DMA_LINK_ALLOCATED_PORT0;
handle_GPDMA1_Channel4.InitLinkedList.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
handle_GPDMA1_Channel4.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_CIRCULAR;
if (HAL_DMAEx_List_Init(&handle_GPDMA1_Channel4) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel4, &List_GPDMA1_Channel4) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(adcHandle, DMA_Handle, handle_GPDMA1_Channel4);
if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel4, DMA_CHANNEL_PRIV|DMA_CHANNEL_SEC) != HAL_OK)
{
Error_Handler();
}
/* ADC4 interrupt Init */
HAL_NVIC_SetPriority(ADC4_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(ADC4_IRQn);
/* USER CODE BEGIN ADC4_MspInit 1 */
/* USER CODE END ADC4_MspInit 1 */
}
}void MX_GPDMA1_Init(void)
{
/* Peripheral clock enable */
__HAL_RCC_GPDMA1_CLK_ENABLE();
/* GPDMA1 interrupt Init */
HAL_NVIC_SetPriority(GPDMA1_Channel4_IRQn, 4, 0);
HAL_NVIC_EnableIRQ(GPDMA1_Channel4_IRQn);
}
2025-10-08 2:43 PM
Hello @AAArdvark ,
the GPDMA is unsecure by default.
You can see GPDMA_SECCFGR that defaults 0, meaning all channels are unsecure.
Same for GPDMA_PRIVCFGR that default value is 0 meaning all channels are unprivileged.
In your code I can see that channels are set secure but privileged is not set. This is probably the reason it fails
Best regards
Jocelyn
2025-10-09 2:51 AM
Hello Jocelyn,
Thank you for your answer; in the code I posted there are these lines:
if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel4, DMA_CHANNEL_PRIV|DMA_CHANNEL_SEC) != HAL_OK)
{
Error_Handler();
}I guess that should set the DMA-channel to secure as well as privileged or am I overseeing something?
Best regards
2025-10-09 10:51 AM
Hello @AAArdvark ,
yes my bad, I missed that.
You say in your post that you set everything secure. So, you confirm that ADC and SRAM are both secure/privilege and GPIOs are also secure ?
I guess you are also using secure alias for buffer address.
Last point, did you enable cache ? But as you say it is working in non secure, this is unlikely the issue.
I would need to reproduce this issue to try finding what happens.
If you can share a code, this would help
Best regards
Jocelyn