cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L496 header missing Hash peripheral definitions

jrgert
Associate III

It looks like STM32L496xx.h does not have the hash peripheral definitions in it. e.g. The STM32Cube_FW_L4_V1.16.0 examples for STM32L496 HASH peripheral are all configured to use the STM32L4A6xx.

Does ST have a plan to update STM32L496xx.h?, or

Is it ST's accepted solution to define the L496 MCU as STM32L4A6xx?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @jrgert​ ,

Thank you for rising this up.

I confirm Jan's answer, the AES and Hash are for crypto only available on STM32L4A6, should not be available on STM32L496.

There are also some wrong notes in the RM0351 which should be fixed (like "HASH available on STM32L49x/L4Ax devices only")

I created an internal ticket (115669) to request correction.

PS: Internal ticket (115669) is not accessible or usable by customers.

Thanks for your contribution.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

3 REPLIES 3
waclawek.jan
Super User

The 'L496 does not have the crypto features, including HASH.

JW

jrgert
Associate III

Well, yeah, I feel dumb. I skipped over the user manual saying "This section applies to STM32L4Ax devices only." :dizzy_face:

I did however open the example project under ...\STM32Cube_FW_L4_V1.16.0\Projects\NUCLEO-L496ZG\Examples\HASH\HASH_SHA224SHA256_DMA

loaded it onto my NUCLEO L496ZG and it works!?

mask error, or undocumented behavior perhaps.

Thanks

Imen.D
ST Employee

Hello @jrgert​ ,

Thank you for rising this up.

I confirm Jan's answer, the AES and Hash are for crypto only available on STM32L4A6, should not be available on STM32L496.

There are also some wrong notes in the RM0351 which should be fixed (like "HASH available on STM32L49x/L4Ax devices only")

I created an internal ticket (115669) to request correction.

PS: Internal ticket (115669) is not accessible or usable by customers.

Thanks for your contribution.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen