2024-09-27 05:18 AM
Hello to all,
I was wondering if there was a way to implement a secure update via USB stick using X-CUBE-SBSFU software.
Moreover, the application software would be installed on external flash, custom bootloader immutable in internal flash.
Maybe installing the new application with my custom bootloader and then letting secure boot do all the security verifications after triggering a system reset?
Sorry if it sounds a silly question but I am quite new to this complex topic.
Thanks!
2024-09-27 06:28 AM
Define secure. What does this mean for you?
2024-09-27 06:45 AM
Hello Pavel,
in my case it means that the new image should be encrypted and decryptable with a secret key, and that I can verify that the image is not corrupted, for example with a SHA256.
Thanks for your time.