cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with reading OBK payload plaintext on STM32H573 using SAES and DHUK

ZhangZhonghao
Associate

I am trying to use the DA function of the STM32H573. I can successfully write the OBK file (with TrustZone disabled) and regression via STM32_Programmer_CLI.exe. However, I encountered an issue when trying to read the plaintext of the OBK payload in my code. I am unable to obtain the correct plaintext through SAES and DHUK.

Here is part of my code:

int32_t OBK_Flash_ReadEncrypted( void *pData)
{
  uint32_t Offset =0x0100;
  uint32_t Length = 0x60;
  uint32_t i = 0U;
  CRYP_HandleTypeDef hcryp = { 0U };
  uint32_t SaesTimeout = 100U;
  uint8_t DataEncrypted[MAX_SIZE] = {0U};
  uint8_t *p_source = (uint8_t *) (FLASH_OBK_BASE_S + Offset);
  uint8_t *p_destination = (uint8_t *) DataEncrypted;
  uint32_t a_aes_iv[4] = {0x8001D1CEU, 0xD1CED1CEU, 0xD1CE8001U, 0xCED1CED1U};


  for (i = 0U; (i < Length); i++, p_destination++, p_source++)
  {
    *p_destination = *p_source;
  }

  __HAL_RCC_SBS_CLK_ENABLE();
  __HAL_RCC_SAES_CLK_ENABLE();

  /* Force use of EPOCH_S value for DHUK */
  //WRITE_REG(SBS_S->EPOCHSELCR, SBS_EXT_EPOCHSELCR_EPOCH_SEL_S_EPOCH);

  /* Configure SAES parameters */
  hcryp.Instance = SAES_S;
  if (HAL_CRYP_DeInit(&hcryp) != HAL_OK)
  {
    return ARM_DRIVER_ERROR_SPECIFIC;
  }
  hcryp.Init.DataType  = CRYP_NO_SWAP;
  hcryp.Init.KeySelect = CRYP_KEYSEL_HW;  /* Hardware unique key (256-bits) */
  hcryp.Init.Algorithm = CRYP_AES_CBC;
  hcryp.Init.KeyMode = CRYP_KEYMODE_NORMAL ;
  hcryp.Init.KeySize = CRYP_KEYSIZE_128B; /* 128 bits AES Key*/
  hcryp.Init.pInitVect = a_aes_iv;

  if (HAL_CRYP_Init(&hcryp) != HAL_OK)
  {
    return ARM_DRIVER_ERROR_SPECIFIC;
  }

  /*Size is n words*/
  if (HAL_CRYP_Decrypt(&hcryp, (uint32_t *)&DataEncrypted[0U], Length / 4U, (uint32_t *)pData, SaesTimeout) != HAL_OK)
  {
    return ARM_DRIVER_ERROR_SPECIFIC;
  }
  if (HAL_CRYP_DeInit(&hcryp) != HAL_OK)
  {
    return ARM_DRIVER_ERROR_SPECIFIC;
  }
  __HAL_RCC_SAES_CLK_DISABLE();

  return ARM_DRIVER_OK;
}
 


I understand that the generation of DHUK is related to many factors, such as SBS_OBK_HDPL, SBS_EPOCH_OUT, and SBS_SEC_NSEC. How should I configure the relevant registers? Or is the DHUK used by RSSLIB not available in user code?

Has anyone done the same thing or encountered the same issue? I would greatly appreciate any answers.

1 REPLY 1
Jocelyn RICARD
ST Employee

Hello @ZhangZhonghao ,

yes this is a known issue. If you do the same with TrustZone enabled it will work.

Issue is that you cannot select proper SAES configuration from your "non secure" firmware.

This issue will be fixed in a future revision of the chip 

Best regards

Jocelyn