cancel
Showing results for 
Search instead for 
Did you mean: 

Debug Authentication Failed

Thatseasy
Associate III

My H5 DK board is in TZ-CLOSED state (after --sfi-flash), I am unable to put it in "Level 1/2/3 Intrusive Non Secure Debug" state no matter what combinations of keys and certificates to use (including key_1_root.pem and cert_root.b64). Only Full regression works. Any suggestions?  Thanks!

 

17:16:50 : Start Debug Authentication Sequence
17:16:50 : SDMOpen : 602 : open : SDM API v1.0
17:16:50 : SDMOpen : 603 : open : SDM Library version v1.1.0
17:16:50 : open_comms : 495 : open : Asserting target reset
17:16:50 : open_comms : 499 : open : Writing magic number
17:16:50 : open_comms : 509 : open : De-asserting target reset
17:16:50 : open_comms : 561 : open : Communication with the target established successfully
17:16:50 : discovery: target ID.......................:0x484
17:16:50 : discovery: SoC ID..........................:0x00000000_35353537_3332510A_003A002B
17:16:50 : discovery: SDA version.....................:2.4.0
17:16:50 : discovery: Vendor ID.......................:STMicroelectronics
17:16:50 : discovery: PSA lifecycle...................:ST_LIFECYCLE_TZ_CLOSED
17:16:50 : discovery: PSA auth version................:1.0
17:16:50 : discovery: ST HDPL1 status.................:0x2717
17:16:50 : discovery: ST HDPL2 status.................:0x400003bf
17:16:50 : discovery: ST HDPL3 status.................:0xffffffff
17:16:50 : discovery: Token Formats...................:0x200
17:16:50 : discovery: Certificate Formats.............:0x201
17:16:50 : discovery: cryptosystems...................:Ecdsa-P256 SHA256
17:16:50 : discovery: ST provisioning integrity status:0xeaeaeaea
17:16:50 : discovery: permission if authorized...........:Full Regression
17:16:50 : discovery: permission if authorized...........:To TZ Regression
17:16:50 : discovery: permission if authorized...........:Level 3 Intrusive Debug
17:16:50 : discovery: permission if authorized...........:Level 2 Intrusive Debug
17:16:50 : discovery: permission if authorized...........:Level 1 Intrusive Debug
17:16:50 : discovery: permission if authorized...........:Level 3 Intrusive Non Secure Debug
17:16:50 : discovery: permission if authorized...........:Level 2 Intrusive Non Secure Debug
17:16:50 : discovery: permission if authorized...........:Level 1 Intrusive Non Secure Debug
17:17:22 : Start Debug Authentication Sequence
17:17:22 : SDMOpen : 602 : open : SDM API v1.0
17:17:22 : SDMOpen : 603 : open : SDM Library version v1.1.0
17:17:22 : open_comms : 495 : open : Asserting target reset
17:17:22 : open_comms : 499 : open : Writing magic number
17:17:22 : open_comms : 509 : open : De-asserting target reset
17:17:22 : open_comms : 561 : open : Communication with the target established successfully
17:17:22 : [00%] discovery command
17:17:22 : [10%] sending discovery command
17:17:22 : [20%] receiving discovery
17:17:22 : [40%] loading credentials
17:17:22 : [50%] sending challenge request
17:17:22 : [60%] receiving challenge
17:17:22 : [70%] signing token
17:17:22 : SDMAuthenticate : 1317 : client : Found 1 certificates
17:17:22 : [80%] sending response
17:17:22 : [90%] receiving status
17:17:22 : Error: Debug Authentication Failed

0 REPLIES 0