2025-12-05 10:28 AM
Hello,
I'm posting a new message because the previous one was not answered with successful connection.
The problem is that when MCU is populated on my board with Read-Our Protection enabled, it is not possible to connect STM32CubeProgrammer v.2.21.0 to that MCU, it becomes a brick.
This option was available in the version 2.0.0. that doesn't work on Windows 11.
How can be done two step connection: 1) full erase and 2) connection ?
Thanks,
Alex
Solved! Go to Solution.
2025-12-05 11:26 AM
You marked an answer in your previous thread. Don't mark an answer if it isn't solved.
Solved: STM32CubeProgrammer connection to MCU that has rea... - STMicroelectronics Community
Why can't you connect to the chip? What happens when you try? Show relevant error messages and screenshots to show the problem.
2025-12-05 11:26 AM
You marked an answer in your previous thread. Don't mark an answer if it isn't solved.
Solved: STM32CubeProgrammer connection to MCU that has rea... - STMicroelectronics Community
Why can't you connect to the chip? What happens when you try? Show relevant error messages and screenshots to show the problem.
2025-12-16 8:00 AM
Hello,
The MCU is soldered on my board and I have access only to UART. The CubeProgrammer v2.21.0 on Windows 11 reports the following error. The old v2.0.0 on Windows 10 allow to make two steps: full erase and connect.
Unfortunately, the version 2.0.0. doesn't work on Windows 11.
Is this option available in CubeProgrammer v2.21.0 ?
Thanks,
Alex