STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

New X-CUBE-SBSFU release

I've heard that the next x-cube sbsfu release would include a fix for the ymodem protocol, such that it can be used from linux, and that it would be released by end of July.Does anybody know when it will be released?

stratom by Associate III
  • 1308 Views
  • 2 replies
  • 0 kudos

I'm trying to initialize an ECDSA 256 public key with the STM32 Crypto library following the example provided in the documentation, but I'm getting the error: ECC_ERR_BAD_OPERATION

EC key information:> openssl ec -in fake_key.pem -text -param_enc explicit -nooutread EC key Private-Key: (256 bit) priv: af:b9:... pub: 04:c0:ae:88:33:3d:a3:d9:ba:20:37:20:05:28:3e: 2a:eb:3e:44:c6:fb:57:08:cd:e4:f4:3e:f9:4d:a6: f0:29...

DGast.1 by Associate III
  • 1450 Views
  • 2 replies
  • 0 kudos

Resolved! XSBSFU package – I still haven't received one download-link

Good evening,I requested the download for XSBSFU package last week , but never received a conformation Email. Today I made another one request and got a conformation Email. I read that it might take up to 48h to get the link, which would be to late f...

EMent.1 by Associate
  • 1452 Views
  • 2 replies
  • 0 kudos

Resolved! APPLI_region_RAM overflow!

Hi... there Hope all are doing well From past few days I'm playing with SBSFU with STM32 L4 Cell-01 Discovery board I'm using x-cube AWS default application with default settings of the linker fileIn demo code, I've added SDMMC with FAT fs, which is ...

0693W000003C5oWQAS.jpg 0693W000003C5obQAC.jpg

Resolved! X-CUBE-SBSFU - no download link yet

Hi!I requested the download on Saturday (sorry - I missed the first mail regarding the setup and was'nt aware of the delay in granting download permission...I started the setup late on Saturday) - I read that it might take up to 48h to get the link, ...

KKreb.1 by Associate
  • 1415 Views
  • 2 replies
  • 0 kudos

Resolved! Firmware security and protection

I've developed an IOT device and now I'm concerned about security. Uses ethernet, tls and mqtt to upload cloud data. Checks a directory on the web for firmware updates. The mqtt is well sanitized and i'm not extremely worried about attack vectors com...

xrstokes by Associate III
  • 4077 Views
  • 7 replies
  • 0 kudos