Skip to main content
b.a.
Associate III
August 5, 2022
Solved

Using STM32L4R5ZI-P without external SMPS, connection to VDD12 pins?

  • August 5, 2022
  • 4 replies
  • 908 views

For a project, I could grab a few STM32L4R5ZI-P µC and am not sure what to connect to the 2 SMPS VDD12 pins when I do not want to provide external voltage but use the integrated LDO.

The datasheet is not quite clear on this scenario.

I have no augmented power saving needs, so the internal LDO will be fine for me.

So, can I just leave pins 70 & 142 floating, or do I have to apply some decoupling capacitors?

Cheers,

B.

This topic has been closed for replies.
Best answer by Bubbles

you can leave the pins floating/unconnected

BR,

J

4 replies

Bubbles
BubblesBest answer
ST Employee
August 5, 2022

you can leave the pins floating/unconnected

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
b.a.
b.a.Author
Associate III
August 8, 2022

Thank you!

M4R10
Associate III
September 13, 2022

Is that valid for SMT32L496VGY also?

When I start debugging with stm32cubeide it goes in 0x1fxxxxx and I can't continue.

M4R10
Associate III
September 15, 2022

Don't cure about it, the problem was a wrong cpu solded on the board