cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to communicate between two Nucleo board using SPI

ercjethava1992
Associate II

I am writing sample demo Application to test data transfer between SPI Master(Nucleo F411RE) and SPI Slavee(Nucleo H755ZI-Q) device.

Master SPI:
/**SPI2 GPIO Configuration
PC2 ------> SPI2_MISO
PC3 ------> SPI2_MOSI
PB10 ------> SPI2_SCK

Slave SPI:
/**SPI1 GPIO Configuration
PA5 ------> SPI1_SCK
PA6 ------> SPI1_MISO
PB5 ------> SPI1_MOSI

For validating what data Slave SPI device receiving over SPI I am sending this data over UART to display it on Host PC 

Here is SLAVE SPI device UART response:
What I am seeing is that SPI receives wrong data instead of 0x41 (Send by master)

 

 

Slave Received SPI data: 0x60 Slave Transmit SPI data: 0xAA Slave Received SPI data: 0x60 Slave Transmit SPI data: 0xAA Slave Received SPI data: 0x60 Slave Transmit SPI data: 0xAA Slave Received SPI data: 0x60 Slave Transmit SPI data: 0xAA Slave Received SPI data: 0x60 Slave Transmit SPI data: 0xAA Slave Received SPI data: 0x60 Slave Transmit SPI data: 0xAA Slave Received SPI data: 0x60 Slave Transmit SPI data: 0xAA

 

 

 


Master SPI Code:

 

 

uint8_t message[1] = {0x41}; int counter = 0; while (1) { HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin); HAL_SPI_Transmit(&hspi2, message, 1, HAL_MAX_DELAY); HAL_Delay(500); counter++; /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } static void MX_SPI2_Init(void) { /* USER CODE BEGIN SPI2_Init 0 */ /* USER CODE END SPI2_Init 0 */ /* USER CODE BEGIN SPI2_Init 1 */ /* USER CODE END SPI2_Init 1 */ /* SPI2 parameter configuration*/ hspi2.Instance = SPI2; hspi2.Init.Mode = SPI_MODE_MASTER; hspi2.Init.Direction = SPI_DIRECTION_2LINES; hspi2.Init.DataSize = SPI_DATASIZE_8BIT; hspi2.Init.CLKPolarity = SPI_POLARITY_LOW; hspi2.Init.CLKPhase = SPI_PHASE_1EDGE; hspi2.Init.NSS = SPI_NSS_SOFT; hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32; hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi2.Init.TIMode = SPI_TIMODE_DISABLE; hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi2.Init.CRCPolynomial = 10; if (HAL_SPI_Init(&hspi2) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN SPI2_Init 2 */ /* USER CODE END SPI2_Init 2 */ }
View more

 

 

 


SLAVE SPI code:

 

 

uint8_t txData[1] = { 0xAA }; // Data to send to the master uint8_t rxData[1] = { 0x00 }; // Buffer to store received data uint8_t tx_uart_buff[50]; while (1) { // Wait for data from the Master if (HAL_SPI_Receive(&hspi1, rxData, 1, HAL_MAX_DELAY) == HAL_OK) { // Data received successfully, respond to master snprintf((char*)tx_uart_buff, sizeof(tx_uart_buff), "Slave Received SPI data: 0x%02X\r\n", rxData[0]); HAL_UART_Transmit(&huart3,tx_uart_buff,sizeof(tx_uart_buff),10); HAL_GPIO_TogglePin(LD1_GPIO_Port, LD1_Pin); // Example: Toggle an LED HAL_SPI_Transmit(&hspi1, txData, 1, HAL_MAX_DELAY); // Send response to the master snprintf((char*)tx_uart_buff, sizeof(tx_uart_buff), "Slave Transmit SPI data: 0x%02X\r\n", txData[0]); HAL_UART_Transmit(&huart3,tx_uart_buff,sizeof(tx_uart_buff),10); } else { snprintf((char*)tx_uart_buff, sizeof(tx_uart_buff), "Slave Receive SPI error\r\n"); HAL_UART_Transmit(&huart3,tx_uart_buff,sizeof(tx_uart_buff),10); } /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } static void MX_SPI1_Init(void) { /* USER CODE BEGIN SPI1_Init 0 */ /* USER CODE END SPI1_Init 0 */ /* USER CODE BEGIN SPI1_Init 1 */ /* USER CODE END SPI1_Init 1 */ /* SPI1 parameter configuration*/ hspi1.Instance = SPI1; hspi1.Init.Mode = SPI_MODE_SLAVE; hspi1.Init.Direction = SPI_DIRECTION_2LINES; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_LOW; hspi1.Init.CLKPhase = SPI_PHASE_1EDGE; hspi1.Init.NSS = SPI_NSS_SOFT; hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLE; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi1.Init.CRCPolynomial = 0x0; hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE; hspi1.Init.NSSPolarity = SPI_NSS_POLARITY_LOW; hspi1.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA; hspi1.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN; hspi1.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN; hspi1.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE; hspi1.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE; hspi1.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE; hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE; hspi1.Init.IOSwap = SPI_IO_SWAP_DISABLE; if (HAL_SPI_Init(&hspi1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN SPI1_Init 2 */ /* USER CODE END SPI1_Init 2 */ }
View more

 

 

 


I have also attached full Master and Slave CubeIDE Project.
If anyone can help me to figure out issue here as SPI Slave always reads wrong data.
@Andrew Neil @tjaekel @Peter BENSCH @B.Montanari 

10 REPLIES 10
ercjethava1992
Associate II

@tjaekel  Master is sending correct data which I have validated based on loopback mode: Master and Slave SPI configuration generated automatically based on STM32CubeMX tool I have provided both Master and SPI configure settings in which you can see NNS settings as SPI_NSS_SOFT which sets that bit which you are referring 

 

 

uint8_t tx_uart_buff[50]; uint8_t message_tx[1] = {0xBB}; uint8_t message_rx[1] = {0x0}; while (1) { if(HAL_SPI_TransmitReceive(&hspi2,message_tx,message_rx,1,HAL_MAX_DELAY) == HAL_OK) { snprintf((char*)tx_uart_buff, sizeof(tx_uart_buff), "Received SPI data: 0x%02X\r\n", message_rx[0]); HAL_UART_Transmit(&huart2,tx_uart_buff,sizeof(tx_uart_buff),10); } else { snprintf((char*)tx_uart_buff, sizeof(tx_uart_buff), "Received SPI Error:\r\n"); HAL_UART_Transmit(&huart2,tx_uart_buff,sizeof(tx_uart_buff),10); } HAL_Delay(500); counter++; /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } // This Master SPI setting generated based on CubeMX IDE which sets CS to SPI_NSS_SOFT Mode void MX_SPI2_Init(void) { /* USER CODE BEGIN SPI2_Init 0 */ /* USER CODE END SPI2_Init 0 */ /* USER CODE BEGIN SPI2_Init 1 */ /* USER CODE END SPI2_Init 1 */ /* SPI2 parameter configuration*/ hspi2.Instance = SPI2; hspi2.Init.Mode = SPI_MODE_MASTER; hspi2.Init.Direction = SPI_DIRECTION_2LINES; hspi2.Init.DataSize = SPI_DATASIZE_8BIT; hspi2.Init.CLKPolarity = SPI_POLARITY_LOW; hspi2.Init.CLKPhase = SPI_PHASE_1EDGE; hspi2.Init.NSS = SPI_NSS_SOFT; hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32; hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi2.Init.TIMode = SPI_TIMODE_DISABLE; hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi2.Init.CRCPolynomial = 10; if (HAL_SPI_Init(&hspi2) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN SPI2_Init 2 */ /* USER CODE END SPI2_Init 2 */ } Received SPI data: 0xBB Received SPI data: 0xBB Received SPI data: 0xBB Received SPI data: 0xBB Received SPI data: 0xBB Received SPI data: 0xBB Received SPI data: 0xBB Received SPI data: 0xBB Received SPI data: 0xBB
View more

 

 


-> I have connected same:

MOSI Master to Slave MOSI 
MISO Master to Slave MISO
SCL Master to Slave SCL

-> I have also verified based on initial code  that If I stop sending data from Master to SLAVE MCU , Slave SPI doesn't receive anything, and when Master sends one byte data to Slave then only Slave receives 1 byte however its wrong byte I am receiving which is an issue I have


# Master
-> SPI Baud Rate = 1.3125 Mbps
-> Full-Duplex Master
-> Hardware control CS : Disabled 

Master-SPI-config.png

Master-Clock-Config.png



# Slave
-> Slave Peripheral Clock Frequency: 5Mz
-> Full-Duplex Slave
-> Hardware control CS : Disabled

SPI-Slave-Config.png


Slave-Clock-Config.png