2025-11-24 11:11 PM
Hello,
I am implementing SPI master communication on an STM32G474RE, transferring 68 bytes per transaction. However, I am unable to achieve the desired SPI clock speed of 5 MHz—currently the SPI clock only reaches approximately 3 MHz.
The system clock is configured at 160 MHz, and I have tested the peripheral clock (PCLK) at both 80 MHz and 160 MHz. Based on these clock settings, I tried multiple SPI prescaler values (16 and 32) to obtain a 5 MHz SCK frequency. In addition, the SPI_SCK pin is configured in High-Speed mode. Despite these settings, the SPI output clock still does not exceed approximately 3 MHz.
Has anyone experienced similar limitations, or is there an additional configuration step required to achieve a stable 5 MHz SPI SCK on the STM32G474RE? Any guidance or suggestions would be greatly appreciated.
Thanks in advance.
2025-11-25 1:03 AM
Hi @RoshiniBejawada,
can you please give me more details about your project so that I can produce your use case? For example, which SPI mode are you using? How did you measure the SPI frequency?
Thanks.
ELABI.1
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-11-25 2:03 AM
Welcome to the forum.
Please give more details of your setup - see: How to write your question to maximize your chances to find a solution
@RoshiniBejawada wrote:Despite these settings, the SPI output clock still does not exceed approximately 3 MHz.
How did you determine that?
What settings, exactly, did you use?