2013-02-22 12:24 AM
Hi everybody,
I'm using a STM32F205VE and something that I don't understand.I do this : USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_Init(USART6,&USART_InitStructure);and I can see the configuration into the USART6 register.I do the same thing for USART3 and nothing happen, no registers are configurated.Have you some ideas about this problem ? Must I do something special for this USART ?Thank you in advance,2013-02-22 12:33 AM
2013-02-22 12:43 AM
For synchronous designs, Rule#1 : Enable the clock.
2013-02-22 12:50 AM
Sorry, I think I will post all my code, it would be easier for everybody.
/* COM1 - NETWORK OUT */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART6, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC,ENABLE); GPIO_PinAFConfig(EVAL_COM1_TX_GPIO_PORT,EVAL_COM1_TX_SOURCE,EVAL_COM1_TX_AF); GPIO_PinAFConfig(EVAL_COM1_RX_GPIO_PORT,EVAL_COM1_RX_SOURCE,EVAL_COM1_RX_AF); /* Configure USART Tx and Rx as alternate function push-pull */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Pin = EVAL_COM1_TX_PIN; GPIO_Init(EVAL_COM1_TX_GPIO_PORT, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = EVAL_COM1_RX_PIN; GPIO_Init(EVAL_COM1_RX_GPIO_PORT, &GPIO_InitStructure); /* Configuration : 115200 bauds, 8 N 1 */ USART_InitStructure.USART_BaudRate = 115200; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; /*USART_OverSampling8Cmd(EVAL_COM1,ENABLE);*/ USART_Init(EVAL_COM1,&USART_InitStructure); /* Enable the USARTx Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = EVAL_COM1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); USART_ITConfig(EVAL_COM1, USART_IT_TXE, DISABLE); USART_ITConfig(EVAL_COM1, USART_IT_RXNE, ENABLE); /* Enable USART */ USART_Cmd(EVAL_COM1, ENABLE); /* Configuration de la PIN REDE */ COMRDInit(COM1); /* COM2 - NETWORK IN */ /* COM1 - NETWORK OUT */ RCC_APB2PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD,ENABLE); GPIO_PinAFConfig(EVAL_COM2_TX_GPIO_PORT,EVAL_COM2_TX_SOURCE,EVAL_COM2_TX_AF); GPIO_PinAFConfig(EVAL_COM2_RX_GPIO_PORT,EVAL_COM2_RX_SOURCE,EVAL_COM2_RX_AF); /* Configure USART Tx and Rx as alternate function push-pull */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Pin = EVAL_COM2_TX_PIN; GPIO_Init(EVAL_COM2_TX_GPIO_PORT, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = EVAL_COM2_RX_PIN; GPIO_Init(EVAL_COM2_RX_GPIO_PORT, &GPIO_InitStructure); /* Configuration : 115200 bauds, 8 N 1 */ USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_Init(EVAL_COM2,&USART_InitStructure); /* Enable the USARTx Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = EVAL_COM2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0F; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0F; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); USART_ITConfig(EVAL_COM2, USART_IT_TC, ENABLE); USART_ITConfig(EVAL_COM2, USART_IT_RXNE, ENABLE); /* Enable USART */ USART_Cmd(EVAL_COM2, ENABLE); /* Configuration de la PIN REDE */ COMRDInit(COM2);2013-02-22 2:04 AM
> RCC_APB2PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);
* =================================================================== * How to use this driver * =================================================================== * 1. Enable peripheral clock using the follwoing functions * RCC_APB2PeriphClockCmd(RCC_APB2Periph_USARTx, ENABLE) for USART1 and USART6 * RCC_APB1PeriphClockCmd(RCC_APB1Periph_USARTx, ENABLE) for USART2, USART3, UART4 or UART5. JW2013-02-22 6:24 AM
Thank you for your answer.
Now my registers are well configured.I'll see if my UART is working !We’re moving the ST Community to a new platform to give you a better and more reliable community experience.