2025-11-18 3:29 AM
I'm using STM32H723ZG
I want to know if a Timer's update event can trigger SPI transfer without any software interrupts.
This is the problem
2025-11-18 4:40 AM
Yes, you can set up a DMA channel to transfer data to/from the SPI on a timer event, such as TRGO.
2025-11-26 11:07 PM
@TDK Can you tell me how to do it step-by-step.
Is this done by DMA Request Synchronization settings?
If it is, for SPI_RX i can see TIM12 TRGO only, and there is no option for setting TRGO event for that timer in MX
2025-11-27 7:34 AM
I don't think this is clickable in STM32CubeMX.
2025-11-27 8:02 PM
then can you show me the other way