cancel
Showing results for 
Search instead for 
Did you mean: 

The stm32 mcus platform has a "Bit Manipulation Engine" similar feature to the NXP mcus platform?

MSpot.2
Associate

Decorated memory store and load for atomic operations

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
TDK
Super User

There are some families with bit-banded SRAM which allows atomic read/write on bits. Not sure if that's what you're looking for or not.

If you feel a post has answered your question, please click "Accept as Solution".
MSpot.2
Associate

Thanks for reply,

I'm aware of bit banding feature that is only for atomic set and clear operation on single bit from alias address to sigle bit.

I want to know if there is such atomic load and store for "and or xor bit-field-extract bit-field-insert" from decorated address usage, e.g. BME in NXP mcus.

Sorry for my english i hope to be clear

Thanks

waclawek.jan
Super User

No.

JW

Uwe Bonnes
Chief

At least GPIO has Bit set and Reset registers for atomic access.