Skip to main content
Tamas Novak
Associate III
December 26, 2014
Question

take care: inverted DEPolarity at LTDC!!

Posted on December 26, 2014 at 13:07

In LTDC_GCR register of LTDC at STM32F429   HSYNC, VSYNC and DE signal polarity may be chosen:

Bit 31 HSPOL: Horizontal Synchronization Polarity

This bit is set and cleared by software.

0: Horizontal Synchronization polarity is active low

1: Horizontal Synchronization polarity is active high

Bit 30 VSPOL: Vertical Synchronization Polarity

This bit is set and cleared by software.

0: Vertical Synchronization is active low

1: Vertical Synchronization is active high

Bit 29 DEPOL: Data Enable Polarity

This bit is set and cleared by software.

0: Data Enable polarity is active low

1: Data Enable polarity is active high

If you set all 3 bits to 0, then VSYNC an HSYNC signals are ''0'', but DE signal will be ''1''.

It's a question of representation: I think the DE signal is ''active'' while sending valuable pixels, and ''not active'' at the time of sync and back/frontporch. ST's representation is different: think of this signal as ''Data Not Valid''.  So

hltdc.Init.DEPolarity = LTDC_DEPOLARITY_AL;  //active low

means that DE signal is 1 while valuable pixels are being sent, and 0 when front+backporch and sync signals active.

    This topic has been closed for replies.