cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4P5 svd file with full TIM15 definition

rdl_42
Associate

Where can I find an svd file for the STM32L4P5 with a full definition for TIM15?

Everything I've found is missing Channel 2 definitions.

Thanks,
-Rob

1 ACCEPTED SOLUTION

Accepted Solutions
Issamos
Associate III

Hello @rdl_42 

You can find the last update of the STM32L4P5 SVD file in the CAD RESOURCES of the STM32L4P5. Or directly using this link.

Best regards.

II

View solution in original post

3 REPLIES 3
Issamos
Associate III

Hello @rdl_42 

You can find the last update of the STM32L4P5 SVD file in the CAD RESOURCES of the STM32L4P5. Or directly using this link.

Best regards.

II

Thanks, that has what I needed.

-Rob

KDJEM.1
ST Employee

Hello @rdl_42 and welcome to the Community 🙂,

I think this FAQ "How to add or update the SVD file in different toolchains: An example using NUCLEO-U575ZI-Q board" can help you to add or update the SVD file in different toolchains.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.