cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L433 NRST pin status

YISHIHARA
Associate II

This is a very basic question.
I built a custom board using the STM32L433.
After applying power (+3.3V), I checked the NRST pin state, but it did not reach the default voltage.
Could you please tell me any possible causes?
For reference, I have confirmed the STM32L433's power pin is at +3.3V. I have also confirmed the clock oscillator is operating at 4MHz.

Thank you in advance.

1 ACCEPTED SOLUTION

Accepted Solutions

You're welcome.

Now, please mark the solution.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

View solution in original post

4 REPLIES 4
Andrew Neil
Super User

welcome to the forum.

Please see How to write your question to maximize your chances to find a solution for best results.

 


@YISHIHARA wrote:

I built a custom board using the STM32L433..


Please show the schematic, your PCB layout, and some good, clear photos.

 

See also: Application note AN4555Getting started with STM32L4 Series and STM32L4+ Series hardware development

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
Super User

> I built a custom board using the STM32L433.

Which one? There are more letters/numbers after this.

If NRST is held low, it generally means the chip is not happy with the power supply. Perhaps you haven't connected ALL VDD pins to power, or not all VSS pins to ground, or part is not oriented correctly, or there are bad connections.

If you feel a post has answered your question, please click "Accept as Solution".

THANK YOU SuperUsers

I confirmed part is not oriented correctly.
And NRST is tured to "H" level.

You're welcome.

Now, please mark the solution.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.