cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 FMC clock configuration

SEMad
Associate III

Hi.

I want to configure a SDRAM in a stm32h743iit6 custom board.

but question is where can I can set the clock of FMC, from below section?

0693W00000HogfxQAB.pngif I set it on 240MHz then the SDCLK Pin supply SDARAM with 240MHz or half of it? or should set with another parameter?

Furthermore the clock frequency of SDRAM is 133Mhz or 143MHz:

0693W00000HogoQQAR.pngbut probably I will force to set the frequency at lower. could it cause any problem?

and finally... what is "SDRAM common clock"?

0693W00000HogzOQAR.pngit should be calculated by tRDD or tCKED or ... ?

0693W00000Hoh3BQAR.png0693W00000Hoh3aQAB.pngsorry for my bad english.

thanks.

3 REPLIES 3
Imen.D
ST Employee

Hello @SEMad​ ,

Please add more details on your post, to increase the chances of getting you a reply from our experts and community members.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".

Hi.

Sorry.

clicked on "ask" inadvertently.

garry lai
Associate II

Why does an error occur when FMC exceeds 100MHz?err01.jpg