2026-05-23 4:10 PM
Hello ST Community,
I've recently updated the firmware for my project to the latest release in CubeMX V6.17.0
I'm using the STM32H743XIH6 device... and the firmware pack was updated to STM32Cube MCU Package for STM32H7 version 1.13.0
When I create a new project, or migrate an older project to this version, I am no longer able to PING my device via ethernet.
I'm utilizing a LAN8720 development board connected via RMII. (USER_PHY selected in CubeMX)
My projects were reliably connecting to the device prior to the firmware package update.
I do notice that there are changes to ethernetif.c with the latest update.
I'm using FREERTOS and LwIP for this build.
Any input on what changes are impacting my project is appreciated.