cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H5 Discovery kit accelerates building secure, smart, connected devices

Amel NASRI
Community manager
Community manager

The STM32H573I-DK is now available for order! It is the first kit to support Secure Manager, a turnkey system-on-chip that integrates core security services certified and maintained by ST.

The STM32H573I-DK enables developers to explore all the integrated features of the STM32H5, such as analog peripherals, timers, the ST ART (Adaptive Real-Time) Accelerator™, media interfaces, and mathematical accelerators. The kit includes all security features, multiple graphics elements, including the color touch display, a digital microphone, as well as several interfaces-USB, Ethernet, and Wi-Fi®.

STM32H5 targets PSA Certified level 3 and SESIP3 certifications. Developers can now speed up the certification process.

Dedicated STM32Cube expansion packages come with this offer, called X-CUBE-AZURE-H5 & X-CUBE-AWS-H5. You can find more about STM32 Cloud Solutions on https://www.st.com/content/st_com/en/ecosystems/stm32-cloud-solutions.html

AmelNASRI_0-1695303865245.png

STM32H5, introduced in March 2023, features the Arm® Cortex®-M33 embedded microcontroller core running at 250MHz and is the first microcontroller to support ST’s Secure Manager system-on-chip security solutions.

 You can find more details about this product on https://www.st.com/content/st_com/en/campaigns/STM32H5-most-powerful-arm-cortex-m33-mcus.html. 

If you have any question or feedback about this product, you can share it with Community. Just pay attention to add STM32H5 Series label.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 REPLIES 2
Sco
ST Employee

👍

Subhan21
Associate

it's very complicated for me you need to research more about this.