STM32G474: Processor hanging when NVIC_Enable Debugger-Timer IRQ.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-12-06 10:09 AM
Hello,
currently I'm transferring from a Nucleo to the target electronics(STM32G474RE3), but when I download the Code(verified successfully) and start it, the Processor is hanging when the Timer IRQ for the Debugger is enabled.
- Supply Voltage is ok, 3.3V
- NRSET is at 3.3V
- Signals on SWDIO and SWCLK look ok(square)
I really have no idea what the issue is, it works on the Nucleo, but it can't get passed that Code.
I'm really running out of ideas, has anyone had these issues before or an idea what the issue may be. The debugger just can not get forward, it's stuck and if I start the controller in standalone, it will not start driving the resonator, driving I2C-Lines,.. nothing.
Thank you everyone in advance for helping.
Best Regards, Seppel
- Labels:
-
Interrupt
-
STM32G4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-12-07 7:03 AM

- « Previous
-
- 1
- 2
- Next »