stm32f769 dsi application problems
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-22 7:41 PM
Dear:
I am working on STM32F769 development board with the dsi unit.
I set the dsi clk to non-continuous mode and set dsi to LP command mode.
Then I inited the dsi module and started the DSI calling the the function HAL_DSI_Start(), there was something wrong with the clk lane. When the function HAL_DSI_Start() is called, sometimes the clk lane went into HS mode but there was no data on the data lane. It does not happen each time.
I don't know why and how to solve the problem or explain it.
Any help would be greatly appreciated. I am looking forward for you reply.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-23 1:07 AM
Hi
cherry.li
,- You are using ST board or a custom board?
- I recommend you to have a look toabout DSI Host on STM32F469/479, STM32F7x8/x9 and STM32L4R9/S9 MCUsA set of example also are provided in STM32F4 cube firmware package :
- STM32Cube_FW_F7_V1.0\Projects\STM32F769I_EVAL\Examples\LCD_DSI
- STM32Cube_FW_F7_V1.0\Projects\STM32F769I_EVAL\Applications\Display\LCD_DSI_ImagesSlider
-Nesrine-
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-24 12:15 AM
Dear:
Thanks for your reply.
I am using ST board. I will have a look to
/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fccc%2Fresource%2Ftechnical%2Fdocument%2Fapplication_note%2Fgroup0%2F1d%2Fb8%2F33%2F4f%2Fdc%2F0a%2F45%2F52%2FDM00287601%2Ffiles%2FDM002876pdf%2Fjcr%3Acontent%2Ftranslations%2Fen.DM002876pdf
and the examples\LCD_DSI carefully again.I have another question here:
The voltage of the gpio is 3.3v. Can I adjust the gpio output volgate to 1.8v? How to make the adjustment?