cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F40G_eval

dorrachendoul
Associate II
Posted on April 15, 2013 at 17:31

STM32F40G-Eval

Hi,

Am having this error,

&sharperror ''Please select first the Evaluation board used in your application (in Project Options)''   

i commented   /* &sharpdefine STM32F427X */ in STM32F44XX.h but i still have this error , how can i fix it.

Thanks

#understand-your-tools
This discussion is locked. Please start a new topic to ask your question.
20 REPLIES 20
Posted on April 16, 2013 at 03:05

Yeah, I'm just working with the cards as dealt, I'm just glad I don't have to support projects concurrently in 4-6 different tool chains.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
dorrachendoul
Associate II
Posted on April 16, 2013 at 10:22

This line of ST Driver was uncommented , thanks for all

dorrachendoul
Associate II
Posted on April 16, 2013 at 10:28

It is still not recognize the GPIO and RCC , that is weird no?

BTW: am using eclipse

frankmeyer9
Associate II
Posted on April 16, 2013 at 10:46

Because you probably omitted to add the path to the respective includes to the include search path in the project settings. Eclipse has a nice GUI for that.

dorrachendoul
Associate II
Posted on April 16, 2013 at 10:57

i went to settings -> arm sourcey linux GCC C compiler ->Directories

and i added this librairies:

''${workspace_loc:/${ProjName}/librarie/CMSIS/Include}''

''${workspace_loc:/${ProjName}/librarie/STM3240_41_G_EVAL}''

''${workspace_loc:/${ProjName}/librarie/Common}''

''${workspace_loc:/${ProjName}/librarie/Device/ST/STM32F4xx/Include}''

''${workspace_loc:/${ProjName}/librarie/STM32F4xx_StdPeriph_Driver/inc}''

''${workspace_loc:/${ProjName}/librarie/STM32F4xx_StdPeriph_Driver/src}''

''${workspace_loc:/${ProjName}/src}''

Isn't like that please?

frankmeyer9
Associate II
Posted on April 16, 2013 at 11:10

In theory, yes.

The following paths are the locations where the std. peripheral drivers (and headers) reside.

... /STM32F4xx_StdPeriph_Driver/inc

.../STM32F4xx_StdPeriph_Driver/src

 

''${workspace_loc:/${ProjName}/librarie/STM32F4xx_StdPeriph_Driver/inc}''

 

''${workspace_loc:/${ProjName}/librarie/STM32F4xx_StdPeriph_Driver/src}''

 

That looks a little suspicious. Is the path name really ''librarie'' ?

And finally, Eclipse generates a full build output, always to a build log file, and to an output console if one is open. Check this output, if the expanded macros and path definitions match your actual path. And if you use Linux, be aware that Linux path/file name are case-sensitive.

dorrachendoul
Associate II
Posted on April 16, 2013 at 11:17

It is me who created the librarie directory and copied the libraries and then when i included the paths i browsed links from  the workspace

dorrachendoul
Associate II
Posted on April 16, 2013 at 11:28

I verified the subdir.mk file of debug and the path match my actual paths

dorrachendoul
Associate II
Posted on April 16, 2013 at 11:53

It is always telling me that the GPIO and RCC could not be resolved, it is workin only when i add in main.c those two includes

# include ''stm32f4xx_gpio.h''

# include ''stm32f4xx_rcc.h''

What is wrong ?

dorrachendoul
Associate II
Posted on April 16, 2013 at 14:46

I fixed the problem i have no errors,

now when i debug i got this:

ledeval_v3 Debug [GDB Hardware Debugging]    

    GDB Hardware Debugger (16/04/13 14:34) (Suspended)    

        Thread [1] (Suspended)    

            2 <symbol is not available> 0x00000000    

            1 <symbol is not available> 0x00000000    

    /home/dorra/CodeSourcery/Sourcery_G++_Lite/bin/arm-none-eabi-gdb (16/04/13 14:34)    

    /home/dorra/workspace/ledeval_v3/Debug/ledeval_v3.elf (16/04/13 14:34)   

and when i oppen the disassembly it is written:

00000000:   Cannot access memory at address 0x0

I can't see what I'm doing wrong here.