cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407 RAM Interface impedance matching

ashutosh211
Associate II

Hi Team,

As we are going to use RAM – IC CY62136EV30 (TSOP-44) in our new project with ST micro STM32F407ZG (LQFP-144).

Do we need any impedance matching for 6-layer board?

Can you please suggest the same. Crystal frequency we taken 16MHz for the MCU.

Thanks.

Regards,

Ashutosh

4 REPLIES 4
TDK
Super User

Having short traces is most important.

Then length matching. Differences up to a couple cm are generally fine.

Then impedance matching. If traces are short, this matters very little.

If you feel a post has answered your question, please click "Accept as Solution".

Thanks for the feedback!

I mean do we need any series resistance (22E or 33E) to be added in data & address line or only shorter distance is enough with length matching on PCB routing? Kindly suggest the same.

ashutosh211
Associate II

Hi Team,

Can you please confirm on above mentioned?

Thanks.

Regards,

Ashutosh

STOne-32
ST Employee

Dear @ashutosh211 ,

You can check our Application Note AN4803

High-speed SI simulations using IBIS and board-level simulations using HyperLynx® SI on STM32 MCUs and MPUs”

all depends on your Frequency speed of clock and data of the RAM I/F. 
Hope it helps you ,

STOne-32