cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CUBE VSCode extension Project setup

Tuomas95
Associate II

Hello,

I'm slightly confused about the options in the STM32CUBE VSCode extension Project setup window.

From the left dropdown i can select the Project, where i have options x, x_AppliSecure, x_AppliNonSecure and x_FSBL, for each of the left options, i can select Secure, Secure-only and Non-secure from the right dropdown for the Security model. I haven't found documentation which describes what do these options mean.

For example, if i select x_AppliSecure from the left dropdown and Non-secure from the right drop down, which sounds like a conflict, what happens? In which scenario should i choose which of the 12 available Project-Security model combinations? Also, I assume that Secure means Secure + Non-secure, as Secure-only must mean secure only and Non-secure probably means Non-secure only?

In the same window, multiple rows can be added to the list from the + button in the bottom right, what do the rows represent?

Tuomas95_0-1765552849297.png

Thanks!

 

0 REPLIES 0