stm32 stop2 mode cannot work when indpendent watchdog enable
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-11-11 1:25 AM
Posted on November 11, 2016 at 10:25
I have an application which enables the watchdog and deepsleep(stop2). The deep sleep mode wakes up by RTC, and then wathcdog is refreshed. However, the MCU still resets by watchdog. I attached code below and I am not sure anything missing by using deepsleep and watchdog.
---------------------------------------------------------------- HAL_Init(); HAL_PWR_EnableBkUpAccess(); /* RTC Clock selection can be changed only if the Backup Domain is reset */ __HAL_RCC_BACKUPRESET_FORCE(); __HAL_RCC_BACKUPRESET_RELEASE(); LSIClock_Config(); __HAL_RCC_PWR_CLK_ENABLE(); /* Ensure that MSI is wake-up system clock */ __HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_MSI); while(1) { refreshDOG(); //this will refresh watchdog, but __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOD_CLK_ENABLE(); __HAL_RCC_GPIOE_CLK_ENABLE(); __HAL_RCC_GPIOF_CLK_ENABLE(); __HAL_RCC_GPIOG_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); GPIO_InitStruct.Mode = GPIO_MODE_ANALOG; GPIO_InitStruct.Speed = GPIO_SPEED_HIGH; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Pin = GPIO_PIN_All; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); HAL_GPIO_Init(GPIOD, &GPIO_InitStruct); HAL_GPIO_Init(GPIOE, &GPIO_InitStruct); HAL_GPIO_Init(GPIOF, &GPIO_InitStruct); HAL_GPIO_Init(GPIOG, &GPIO_InitStruct); HAL_GPIO_Init(GPIOH, &GPIO_InitStruct); __HAL_RCC_GPIOA_CLK_DISABLE(); __HAL_RCC_GPIOB_CLK_DISABLE(); __HAL_RCC_GPIOC_CLK_DISABLE(); __HAL_RCC_GPIOD_CLK_DISABLE(); __HAL_RCC_GPIOE_CLK_DISABLE(); __HAL_RCC_GPIOF_CLK_DISABLE(); __HAL_RCC_GPIOG_CLK_DISABLE(); __HAL_RCC_GPIOH_CLK_DISABLE(); /* Disable all used wakeup source */ HAL_RTCEx_DeactivateWakeUpTimer(&RTCHandle); HAL_RTCEx_SetWakeUpTimer_IT(&RTCHandle, 0x03FFF, RTC_WAKEUPCLOCK_RTCCLK_DIV16); /* Enter STOP 2 mode */ HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI); /* Re-configure the system clock to 80 MHz based on MSI, enable and select PLL as system clock source (PLL is disabled in STOP mode) */ SYSCLKConfig_STOP(); } #watchdog-deepsleep
Labels:
- Labels:
-
Power
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0