2014-10-06 8:36 AM
2014-10-06 10:23 AM
Is your example codes for stm32f4 Discv. Board ?
It says so doesn't it? Assumeshttp://www.st.com/web/en/catalog/tools/PF257904
is being used, and you have a suitable serial connection wired up.2014-10-06 10:40 AM
Mr clive thanks for the code,
I put the project under: \stm32f4\STM32F4xx_DSP_StdPeriph_Lib_V1.4.0\Project\F4DISCO_USART2HELLO Not usedhttp://www.st.com/web/en/catalog/tools/PF257904
buthttp://www.st.com/web/en/catalog/tools/PF257904
; and used just one pin PA2 as TX with this cable : http://www.aliexpress.com/item/New-USB-to-RS232-COM-Port-Serial-PDA-9Pin-DB9-Cable-Adapter/607153241.html Here is my hello world : «::.ú‹….'7½ë2014-10-06 10:57 AM
The STM32 does not output RS232 compatible voltages.
http://www.amazon.com/PL2303HX-RS232-Cable-Module-Converter/dp/B008AGDTA4
2014-10-06 11:03 AM
http://www.maximintegrated.com/en/products/interface/transceivers/MAX3232.html
2014-10-06 11:07 AM
Thats why. I confused; so sorry.Thanks Mr Clive, appreciate your help and all your effort.