cancel
Showing results for 
Search instead for 
Did you mean: 

ST-LINK Cannot Detect Target – NUCLEO-F072RB – “Unable to get core ID” / “No STM32 target found”

Visu
Associate II

Hi,

I am facing an issue while connecting to my board using STM32CubeProgrammer and ST-LINK. I would appreciate any help.

Board: NUCLEO-F072RB
Programmer: ST-LINK (Onboard)
Software: STM32CubeProgrammer
Connection: SWD
ST-LINK Firmware: V2J46M31

Issue Description:
STM32CubeProgrammer is unable to detect the target MCU. It shows errors like:

  • Unable to get core ID

  • No STM32 target found

  • ST-LINK error (DEV_CONNECT_ERR)

Observed Details:

  • Target voltage showing around 0.29V

  • Connection mode tried: Normal (SWD)

  • Reset mode: Software reset

  • Speed: Reliable

  • Frequency: 4000 kHz

Log Messages (Important Parts):

  • Error: Unable to get core ID

  • Error: No STM32 target found!

  • ST-LINK error (DEV_CONNECT_ERR)

  • Error: Problem occurred while trying to connect

What I Already Checked:

  • USB cable and port

  • Reinstalled STM32CubeProgrammer

  • ST-LINK firmware upgrade option checked

  • Tried reconnecting multiple times

Questions:

  1. Is the low target voltage (0.29V) the reason ST-LINK cannot detect the MCU?

  2. Could this be a power supply or hardware issue on the board?

  3. Should I try different reset modes (Hardware reset / Connect under reset)?

  4. Any recommended debugging steps for this case?

Thanks in advance for your support.

0 REPLIES 0