cancel
Showing results for 
Search instead for 
Did you mean: 

SPI Bootloader with micro at lower voltage

Caveman
Associate II

I have two different STM32L451 boards.

One version runs at 3.3V and the other at 1.95V.

On the 3.3V board, I can enter the SPI Bootloader and erase/program Flash reliably.

But on the 1.95V board, the flash write fails. In the same 2K page and on usually the same 256-byte block, I fail to get an ACK after sending the write command.

I have the same issue on two L431 boards as well.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
MM..1
Chief III

Is your SPI connected too 1.95V ? You try other SPI speeds?