cancel
Showing results for 
Search instead for 
Did you mean: 

Setup for CAN-FD communication with NUCLEO-H7A3ZI-Q

NStei.2
Associate II

Hello good day!

I want to setup a CAN-FD message sending simulation with H7A3ZI-Q (one or two message ids). But i do not exactly know how to assemble the HW and what i need (For STM side). I know this board is capable of the CAN-FD but it needs a tranceiver. Is there already a board i can use for Pin PD0 and PD1 are the outputs of the CAN controller i want to connect.

For example I found this:

CAN FD 5 CLICK MIKROELEKTRONIKA - Click board | Transceiver; UART; UJA1162A; Prototypenplatine; MIKROE-4286 | TME - Elektronik Bauteile -> Where do I have to connect the RX/TX CAN output of the STM (5V+GND I would supply also)?

or a better alternative this:

CAN-Bus CAN FD Breakout Board. 5v Supply and 5v Logic (buyzero.de) -> here it is "just the TX and RX" to be connected.

Any advice from you experts?

Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
NStei.2
Associate II

Can be closed - solved.