2025-01-08 4:50 AM - last edited on 2025-01-08 4:57 AM by Andrew Neil
What is the reference voltage did ST set in STM743 micro controller for temperature sensor for acquiring the Calibrated value TSCAL2 & TSCAL1 for 130*C and 30*C. Since during factory set How do ST Know What external voltage is going to come from design side ?
For Example If you set reference voltage 1.2V for 130*c then How do i scale it that if i give 2.5V external voltage for Vref ? Then calibrated value i am getting from internal is different from what i am expecting so it will throw error in calculation ? How do i know the information about factory set Ref voltage for TSCAL2 and TSCAL1 for maximum and minimum temperature ?
Is there any application note for calculating the temperature as per the reference voltage to get to know the internal calibrated value for TSCAL2 & TSCAL1 ?
2025-01-08 4:47 AM - last edited on 2025-01-08 5:45 AM by mƎALLEm
Merging of two thread for the same subject.
what is the maximum temperature did set in STM743 micro controller during factory set for TS_CAL2 Calibrated value? Is it 110*c or 130*C for maximum temperature Calibrated value ?
Since STM743 Production Datasheet Rev 7, Table 191 shows for 110*C but in Rev10 shows 130*c for TS_CAL2. The given memory address is same for both revisions so i will get only one data under that
Rev7 STM743 Reference Document RM0433 in Section 25.4.33
Temperature (in °C) = 110 °C – 30 °C
-------------------------- × (TS_DATA – TS_CAL1) + 30 °C
TS_CAL2 - TS_CAL1
Rev8 STM743 Reference Document RM0433 in Section 25.4.33
Temperature (in °C) = TS_CAL2_TEMP – TS_CAL1_TEMP
------------------------------------------------------- × (TS_DATA – TS_CAL1) + 30 °C
TS_CAL2 - TS_CAL1
so I want to know that whether it is for 110*c or 130*c for max temperature Calibrated value.
2025-01-08 5:55 AM
What is the reference voltage for the internal temperature sensor this ti connected with internal ADC ?
2025-01-08 7:20 AM
The datasheet says it's 110 C for rev Y and 130 C for rev V. Presumably, the RM was changed due to it varying between revisions.
2025-01-08 7:22 AM
The reference voltage for these readings is 3.3V +/- 10 mA.
2025-01-08 9:59 PM
Ok Thank you. What is the meaning of RM ? may i Know ?
2025-01-08 10:01 PM
So What is the max temperature did set in for the controller for TSCAL2 during calibration? 110* c or 130*c ?
2025-01-09 7:29 AM
Reference Manual.
2025-01-09 7:34 AM
> So What is the max temperature did set in for the controller for TSCAL2 during calibration? 110* c or 130*c ?
As I said before:
> The datasheet says it's 110 C for rev Y and 130 C for rev V.
To find out what chip revision you have, connect to it with STM32CubeProgrammer and look in the bottom right. Typically, you will have the newer revision (V).
2025-01-09 10:27 AM
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.