cancel
Showing results for 
Search instead for 
Did you mean: 

Programming STM32WB15CCU6E in Arduino IDE

mhcheng
Associate

I am trying to program my custom board with STM32WB15CCU6E on it in Arduino IDE. I always upload the code to my nucleo-wb15 board to verify if it is working before uploading it to the custom board. The main difference between the chip used on nucleo-wb15 and STM32WB15CCU6E is that my custom board has no external 32.768 kHz crystal installed, so it mainly relies on HSE or LSI.

However, I could not make my BLE module advertise on my custom board while it is working fine on the nucleo-wb15. I am suspecting except the Arduino code, I probably need to change something in the variant file. Anyone knows how to do it? thanks.

1 REPLY 1
Issamos
Lead III

Hello @mhcheng

I think this is not the right place for questions on the STM32duino. I suggest you to report this issue on the STM32duino repo . You can also report it her https://www.stm32duino.com/ but it is not working for me. @Imen.D  Could you please check the issue on the website.

Best Regards.

II