2026-01-16 9:36 AM
Hi everyone,
I’m trying to get the LwIP examples from the stm32-hotspot GitHub (this one: https://github.com/stm32-hotspot/STM32H7-LwIP-Examples) running on my NUCLEO-H723ZG, but I’m hitting a wall.
The README is actually great and super clear, which is why I’m surprised I can’t get it to work. I’ve built the project and flashed it to the board, and I have it connected directly to my laptop via Ethernet.
The docs say the IP should be 192.168.1.10, but when I try to ping it, I get nothing. I also took a look at the code and it looked like the IP might be set to 192.168.1.1 instead, so I tried pinging that too, still no luck.
Am I missing something basic here? Is it enough to just build and flash the code, or do I need to tweak some jumpers on the Nucleo or change my laptop's manual IP settings to be on the same subnet?
I’d really appreciate it if someone who has used this repo could point me in the right direction.
Thanks!
mpek29