cancel
Showing results for 
Search instead for 
Did you mean: 

Nor Flash memory mapping works unexpected on P-NUCLEO-WB55

Charles_Li
Associate II

I'm using MX25V1635F on WB55

Below, read/write functions work fine

#define SECTOR_ERASE_CMD 0x20
#define QUAD_IN_FAST_PROG_CMD 0x38

But in memory mapping mode, only few bytes correctly or even nothing right,

CS, SCLK work as expected but D0 seems like out of control, is there any idea?

2 REPLIES 2
Roger SHIVELY
ST Employee

Hello @Charles_Li ,

There has been a case created to resolve this question and we will be reaching out to you directly.

Regards,
Roger

The code for the working read/write would be helpful, along with the not working memory mapped template.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..