2024-08-31 03:12 AM
I've successfully implemented a small machine learning model on the STM32F303ZE, and it's working well so far. However, I’m curious about the maximum size of the model that this microcontroller can handle. Has anyone experimented with larger models on the STM32F303ZE? What are the limitations in terms of model size, and at what point should I consider switching to another board?