cancel
Showing results for 
Search instead for 
Did you mean: 

Interleaved peak current control channels using slope compenstation on Nucleo-F334R8

decook1110
Associate

Could someone clarify if the Nucleo-F334R8 boards can operate two interleaved channels with using peak current mode control, each channel would need its own slope compensation.  I understand the board can do a single phase and has 3 DACs, but I see it has only one internal op-amp.  I'm still on the steep part fo the learning curve here. We're stepping up from simpler analog voltage mode control and I'd really like to insure this board by itself will do that job or if we need a more powerful board to do both channels with one controller.  -- Thanks

1 REPLY 1
decook1110
Associate

As I started down the path of looking into using MCU's in power electronics, I was told I'd find the forum support at ST better than that for TI. 

I believed this was a pretty easy question for people who are familiar with these systems, am I asking it on the wrong forum??