Skip to main content
shane mattner
Senior
September 6, 2023
Solved

HSE Oscillator for STM32L01 series MCU

  • September 6, 2023
  • 4 replies
  • 1588 views

I'd like to try using the STM32L011E4Y6TR in a new design.  However, the HSE input has only one pin (RCC_CK_IN) and I'm not sure how to use it with a standard 4 pin crystal that typically connects to 2 mcu pins.  Can someone point me toward a reference design oscillator circuit for the STM32L0 series?

This topic has been closed for replies.
Best answer by Foued_KH

Hello @shane mattner , 

You can't connect a crystal/Ceramic Resonator as HSE for this package ( pins limitation)
The only way to use HSE is to inject a signal through the PA0.
Or you can connect a crystal/Ceramic Resonator  as LSE through PC14 and PC15.

Hope it helps!

Foued

4 replies

Issamos
Super User
September 6, 2023

Hello @shane mattner 

This post may answer your question.

Best regards.

II

Foued_KH
ST Employee
September 6, 2023

Hi @Issamos , 

The STM32L011E4Y6TR package is WLCSP25 not the LQFP32 

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Issamos
Super User
September 6, 2023

Hello @Foued_KH 

Thanks :smiling_face_with_smiling_eyes:

 

Foued_KH
Foued_KHBest answer
ST Employee
September 6, 2023

Hello @shane mattner , 

You can't connect a crystal/Ceramic Resonator as HSE for this package ( pins limitation)
The only way to use HSE is to inject a signal through the PA0.
Or you can connect a crystal/Ceramic Resonator  as LSE through PC14 and PC15.

Hope it helps!

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.