Skip to main content
BPart.1
Associate II
October 24, 2025
Solved

HSE Bypass mode - Possible use of OSC_OUT as GPIO

  • October 24, 2025
  • 3 replies
  • 360 views

Hi I am looking into using STM32F446RCTx for my design, which includes 2 x USB FS 2.0 (1 x Host + 1 x Device). Hence need to provide an external HSE. I want to use an Oscillator, meaning I setup the HSE as "Bypass Clock Source" .

With this setup I planned to use the pin 6 (PH1_OSC_OUT) as a GPIO for other functionalities. But the STM32CubeMX setting does not let me do this.

I see that this pin will be (OSC_OUT) High Impedance as per RM0390 - Page 120. Am I right in say that I MUST leave this pin NC and cannot free up to use as GPIO?

Thanks.

 

 

Best answer by mƎALLEm

Hello,

I've got a confirmation from the team: yes for STM32F446 you can use OSC_OUT and OSC32_OUT as GPIOs when HSE or LSE are in bypass mode.

The documentation will be updated accordingly (Internal ticket number 220390).

Hope that answers your question.

3 replies

mƎALLEm
ST Technical Moderator
October 24, 2025

Hello,

I think that possibility is available only in newer products. STM32H7 can do that.

According to the STM32F446 reference manual. It says not. But I can check internally. Internal ticket number 220390 not accessible by the community members.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
BPart.1
BPart.1Author
Associate II
October 24, 2025

Hi Thanks for checking this out. 

waclawek.jan
Super User
November 18, 2025

> yes for STM32F446 you can use OSC_OUT and OSC32_OUT as GPIOs when HSE or LSE are in bypass mode

This is interesting. I've just tested and, yes, the 'F446 is different from the 'F427 (and thus presumably also 'F407) in this detail.

I've noticed another interesting and undocumented detail: in both the 'F446 and the 'F427, the RCC_CR.HSEBYP bit appears to be not reset by Software Reset, only by NRST and Power Reset.

JW

Andrew Neil
Super User
November 29, 2025
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.