cancel
Showing results for 
Search instead for 
Did you mean: 

How to use CCMRAM ? in my STM32F746G board

Mani1
Associate II

Board : STM32F746G

How to use CCMRAM?

What is the use CCMRAM?

What is the Size of CCMRAM?

Thanks

Manikandan D

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
TDK
Super User

How to use:

https://www.openstm32.org/Using%2BCCM%2BMemory

However, the STM32F7 doesn't have CCMRAM.

For boards that have it, CCMRAM provides faster memory access compared to other SRAM.

The STM32F7 has DTCM RAM which can be used in a similar fashion and has effectively the same benefits (faster access) and drawbacks (can't be accessed by DMA) as CCMRAM.

The DTCM RAM is 64kB and is located at 0x20000000. This info is found in the reference manual.

If you feel a post has answered your question, please click "Accept as Solution".
Mani1
Associate II

Thank you soo much @TDK​ 

> drawbacks (can't be accessed by DMA)

It should be noted that the F7 series is an exception to this as all DMAs can access DTCM memory through the AHBS bus. Similarly on H7 MDMA can access DTCM and ITCM memories through the AHBS bus.