cancel
Showing results for 
Search instead for 
Did you mean: 

How the H750 kernel is powered using an external power supply

allgoodhi
Associate II

When using the STM32H750VBT6, I supplied around 1.37-1.4 supply voltage to the external pins VCAP1 and VCAP2,the project was configured as an external power supply using cubemx software.HAL_PWREx_ConfigSupply(PWR_EXTERNAL_SOURCE_SUPPLY); is used in the program.Frequency automatically configured to 480 MHz via cubemx (internal clock source).

allgoodhi_0-1715329182041.png

allgoodhi_0-1715328294289.png

According to the manual said burned into the power-off restart, and then to be effective, after the start may not be able to recognize the chip can not be debugged, good luck may be debugging, but run for a while will enter the Hardware Error Interrupt Function in the HardFault_Handler().How to solve this problem.

 

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Super User

>supplied around 1.37-1.4

"around" is not adequate definition here ; :)

+

this is core supply , maybe 200mA needed; so  R48/49 = 0. 

And Vcap low noise, low impedance source !

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
AScha.3
Super User

>supplied around 1.37-1.4

"around" is not adequate definition here ; :)

+

this is core supply , maybe 200mA needed; so  R48/49 = 0. 

And Vcap low noise, low impedance source !

If you feel a post has answered your question, please click "Accept as Solution".

Voltage fixed at 1.375V,Do you mean to use 0R resistors for R48 and R49?

切换到 0R 解决了它,谢谢