cancel
Showing results for 
Search instead for 
Did you mean: 

half-duplex spi slave can't transmit datas

Jseyn.1
Associate III

i used stm32f031 as master & slave, NSS is alwasy low, connect MOSI and MISO. the master transmit datas successfull then changing the master direction to receive data( SPI->CR &=~SPI_CR1_BIDIOE), at the same time slave recv and try to transmit datas.

here is the master code:

for(i = 0; i < 256; i++)

{

while((SPI1->SR & SPI_SR_TXE) != SPI_SR_TXE);

SPI1->DR = i;

delay_us(10);

}

delay_ms(2);

SPI1->CR1 &= ~SPI_CR1_BIDIOE;

delay_ms(3);

for(i = 0; i < 256; i++)

{

while((SPI1->SR& SPI_SR_RXNE) != SPI_SR_RXNE);

master_rx_16[i] = SPI1->DR;

}

delay_ms(2);

i find no data in master_rx_16[].

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0