cancel
Showing results for 
Search instead for 
Did you mean: 

Error: target voltage may be too low for reliable debugging

AhmedSayed
Associate II

i separated the debugger of my nucelo stmf401re from the rest of the board and i am using it to debug an stm32h750
but when i try to connect it with cube id i get those messages:
Open On-Chip Debugger 0.12.0-00017-gb153daa14 (2023-02-03-14:58) [https://github.com/STMicroelectronics/OpenOCD]
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J41M27 (API v2) VID:PID 0483:374B
Info : Target voltage: 0.012615
Error: target voltage may be too low for reliable debugging
Error: init mode failed (unable to connect to the target)

the debugger is detected normally on the ide .
 i think there is a connection that i should make after breaking the debugger from the rest of the board is that right, and if so, what is it??


2 REPLIES 2
FBL
ST Employee

Hello @AhmedSayed 

Check the connections to the debugger. Try using CubeProgrammer to make sure the issue is not related to OpenOCD.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

AScha.3
Chief

target voltage ...st-link want to know voltage here. try connect cn2 pin1 to vcc 3v3 on your target.

AScha3_0-1688400093355.png

 

If you feel a post has answered your question, please click "Accept as Solution".