cancel
Showing results for 
Search instead for 
Did you mean: 

Clarification on Clock Source Selection for STM32U575CGU3 in CAN J1939 & CANopen Application

sasmitjoshi5
Associate II

I am currently working on a project that uses the STM32U575CGU3 microcontroller. The goal of the project is to display pressure and temperature values over CAN J1939 and CANopen communication protocols in a digital output format.

For sensor data acquisition, I am using an external two-channel ADC to measure pressure and temperature values.

Regarding the system clock, I have tested the application using both the internal clock source and an external crystal oscillator. The system performs well in both configurations.

However, I would like to request your expert guidance on the recommended clock source for this application. Specifically:

  • Is it advisable to use the external crystal for better timing accuracy and long-term stability?
  • Or is the internal clock sufficiently reliable for CAN J1939 and CANopen communication in a production environment?
1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello @sasmitjoshi5 and welcome to the ST community.

No matter CANOpen is used or not. It's recommended to use a Crystal with CAN/FDCAN especially for industrial environment otherwise you will face some communication issues.

See also: Do I need an external crystal for RS485 or CAN on STM32H533RET6?

Hope I've answerd your question.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
mƎALLEm
ST Employee

Hello @sasmitjoshi5 and welcome to the ST community.

No matter CANOpen is used or not. It's recommended to use a Crystal with CAN/FDCAN especially for industrial environment otherwise you will face some communication issues.

See also: Do I need an external crystal for RS485 or CAN on STM32H533RET6?

Hope I've answerd your question.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.