STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 Discovery board to PC interface

Posted on November 25, 2015 at 06:23Hi everyone,I just want to seek your guidance and help in accessing 12 signed 32 bit integers, which are calculated by using STM32F4 Discovery board, in my PC, through USB.I read many codes/post on different forum...

waheed901 by Associate II
  • 2271 Views
  • 4 replies
  • 0 kudos

USB with Cube.

Posted on January 29, 2016 at 08:14Hi. I have been playing with Cube for the Nucleo F1 series, and I'm interested in getting a USB app running. I know a little about HID, and I can create a HID cube project for SW4STM32 and it enumerates as a HID. T...

kvresto by Senior
  • 2002 Views
  • 5 replies
  • 0 kudos

Flash memory driver

Posted on January 31, 2016 at 22:24I'm working my way through AN4061:http://www.st.com/web/en/resource/technical/document/application_note/DM00049914.pdfUnder section 2.3, it says ''This section describes the driver implemented for the EEPROM emulat...

joe2399 by Associate II
  • 1689 Views
  • 2 replies
  • 0 kudos

[F030] Using ADC with DMA and multiple channels

Posted on January 30, 2016 at 13:38hello allI need advice about using the ADC embedded in the STM32F03. I am connecting 5 analogue sources which I want to acquire with different rateS0 every 2nd sampleS1 every 3rd sampleS2 every 6th sampleThe idea i...

stanzanim by Associate III
  • 861 Views
  • 2 replies
  • 0 kudos

interfacing between different boards

Posted on January 30, 2016 at 06:42I got a NUCLEO-F446RE, which I use to send control signal to other board via SPI and GPIO. The NUCLEO and the board are powered separately. I wonder do I have to put them to the common ground so to make them work?

llwaeva by Associate II
  • 1201 Views
  • 2 replies
  • 0 kudos

Multiple Channel ADC on STM32 L1 Discovery with CooCox

Posted on January 29, 2016 at 13:46Hello STM users,I have been thrown in 'at the deep' using an STM32L152 in a commercial product design. I have inherited some code which uses the CooCox CooIDE for development and an STM32 L1 discovery board which u...

cht35 by Associate II
  • 3577 Views
  • 15 replies
  • 0 kudos

problem using STM32F407 FSMC with NOR flash

Posted on January 28, 2016 at 09:53Hi all,I am trying to interface with JR28F064M29EW NOR flash (https://www.micron.com/~/media/documents/products/data-sheet/nor-flash/parallel/m29ew/m29ew_32mb_128mb.pdf) using the STM32F407 MCU. However, I couldn't...

minh3192 by Associate II
  • 2053 Views
  • 4 replies
  • 0 kudos

STM32Fxx USART application bootloader

Posted on January 29, 2016 at 05:07I am writing an application bootloader for stm32f4xx. What is the best way to detect end of transmission over serial line? #!stm32f4-!stm32f401

nus by Associate
  • 2064 Views
  • 6 replies
  • 0 kudos

Pin PA8 configured as OUTPUT

Posted on January 29, 2016 at 16:30 Hello, I'm trying for several days to set up the pin PA8 ( STM32F4) as output but I do not see anything with an oscilloscope. Here is the code I use ...

guigui by Associate II
  • 4070 Views
  • 5 replies
  • 0 kudos